--------------------------------------------------
                   Driver Installer/Uninstaller v3.4/3.4 Release Notes
                     Copyright (C) 2013 Silicon Laboratories, Inc.
		 --------------------------------------------------


This release contains the following components:

   * DriverInstaller.exe - Installation executable with embedded uninstaller. These executables
	are paired for installation of Silicon Labs driver sets. The uninstaller executable is
	embedded within the DriverInstaller.exe and are extracted during the driver installation
	to the installed directory (if it exists, if not it is copied to a standard Silicon
	Labs directory). The DriverInstaller.exe is driven by a setup.ini file which contains all
	the customization for the installation and install/uninstall modes.

   NOTE: This package contains the latest executable for use with a driver set. Simply drop in and
	replace the older installation EXE in your customized driver set. Rename the EXE file to your
	desired setup name, and it will be ready to run.


Known Issues and Limitations
----------------------------

	1) Supported operating systems: 2000\XP\Server2003\Vista\Windows7


Release Dates
-------------

	Driver Installer/Uninstaller 3.4/3.4 - Oct 14, 2011
		*Updated April 18, 2013 with valid Silabs Verisign Certificate	



Revision History
-----------------

Installer Version 3.4 /
Uninstaller Version 3.4

	Bugs Fixed
	----------
	- Corrected the requirement to have to right click to Run As Administrator introduced
	in version 3.3 for Vista/7.

Installer Version 3.3 /
Uninstaller Version 3.3

	Bugs Fixed
	----------
	- Corrected uninstallation issue when more than 23 devices are referenced in
	the installation package. Now the maxiumum number of supported devices per installation
	is 40.

Installer Version 3.2 /
Uninstaller Version 3.2

	Bugs Fixed
	----------
	- Corrected uninstallation bug seen when upgrading from older driver versions
	using older (pre 2.8) installer versions

Installer Version 3.1 /
Uninstaller Version 3.0

	Bugs Fixed
	----------
	- Corrected uninstallation bug when performing a copy only installation

Installer Version 3.0 /
Uninstaller Version 3.0

	New Features
	------------
	- Added support for multiple VID and PIDs to be included in a single installation
	- Added option to specify a specific INI file with the -ini command line option

	Bugs Fixed
	----------
	- Modified the number of INF files looked at during the preinstall check to speed
	up the installation process as much as possible


Installer Version 2.8 /
Uninstaller Version 2.6

	Bugs Fixed
	----------
	- Corrected an error in the process for a "non-copy" install
	- Corrected an error where the uninstaller is incorrectly extracted during a silent
	installation


Installer Version 2.7 /
Uninstaller Version 2.6

	Bugs Fixed
	----------
	- Corrected problem in installation that caused incorrect directory to be
	listed in the regsitry to reference the uninstaller, which would cause error
	on uninstallation


Installer Version 2.6 /
Uninstaller Version 2.6

	Bugs Fixed
	----------
	- Updated to now use the install or program files directory for the uninstaller
	since the system directory is protected.
	- Made installer more robust, if it finds a driver with no preinstaller (such as
	Windows removing it) it will create one to remove the previous driver.
	

Installer Version 2.5 /
Uninstaller Version 2.5

	New Features
	------------
	- Updated to remove the Uninstaller from the system upon successful uninstall
	- Added Publisher, InstallLocation and Version keys to the uninstallation key
	for Add/Remove Programs


Installer Version 2.4 /
Uninstaller Version 2.4

	New Features
	------------
	- Updated to include relative installation support for language specific and
	user defined Program Files directories and relative installation support to the
	Windows driver.
	- Added a sample INI file to the package


Installer Version 2.3 /
Uninstaller Version 2.2

	New Features
	------------
	- Updated so that when a device is plugged in and "ignored" (user clicks "Don't
	ask me again" when choosing not to install a driver for a device) the installer
	will remove and rescan those hardware IDs so the device will install


Installer Version 2.2 /
Uninstaller Version 2.2
---------------------

	Bugs Fixed
	----------
	- Added privilege checking to the start of the Install/Uninstall process

	- Added removal of Add\Remove Programs key from registry upon failure of
	uninstallation

	- Fixed uninstallation failure when using Device Manager to remove the device
	install before using the Add\Remove programs entry in Vista


Installer Version 2.0 /
Uninstaller Version 2.0
---------------------

	New Features
	------------
	- Updated to include Vista support.
	
	- Updated to allow subdirectories to be supported for installation.


Installer Version 1.5 /
Uninstaller Version 1.5
---------------------

	Bugs Fixed
	----------
	- Changed the process of generating an uninstaller for both XP/2K3 or 2K and now
	only generate a single OS non-specific uninstaller.	


Installer Version 1.4 /
Uninstaller Version 1.4
---------------------
	
	Bugs Fixed
	----------
	- Fixed issue of installing "read-only" files. Error messages are no longer displayed, and
	the application will allow read only files to be copied over or deleted. This applies to
	copying within the DriverInstaller.exe and deletion within the DriverUninstaller.exe.


Installer Version 1.3 /
Uninstaller Version 1.1
---------------------
	
	New Features
	------------
	- Added Update support into the installer so that drivers existing on the system
	that have been installed with this software can be updated.	


Installer Version 1.2 /
Uninstaller Version 1.1
---------------------
	
	New Features
	------------
	- Catalog files can be specified in the INF even if they are not present. An
	error is no longer generated when the copy fails because they are missing. This
	should make testing easier before WHQL certification is done, and the support for
	copying the Catalog files exists so that they can just be dropped into the installation.

	
Version 1.1
-----------

	New Features
	------------
	- Added support for ignoring serial numbers


Version 1.0
-----------

	Initial Release